Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the padlock attachment for the electrically operated P frame breaker?
Issue:
Is there a padlock attachment option available for the motor operated PowerPacT P-frame breaker?

Product Line:
Motor Operated Breakers

Resolution:
The motor operated P frame breaker comes with a padlock OFF option standard.
It can also be replaced by field installable padlock attachment S47514.
A Kirk keylock provision is also available, part number S47517.  For provision and lock, order S48939.
Thee electrically operated P frame can have the padlock attachment OR the keylock--not both.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings