Issue:
Do electrically operated Powerpact P frame breaker comes with opening and closing coils?
Product Line:
Powerpact P frame breaker
Resolution:
Yes, electrically operated (motor operated) Powerpact P frame breakers come with open and close coils with the same voltage rating as the motor.
Note: If you have a motorized Powerpact P frame and replace the motor with one of a different voltage, you also need to order open and close coils of the same voltage as the new motor per the following table:
Released for: Schneider Electric Canada