Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to mount the S33576MK neutral CT mounting kit and S33576 neutral CT onto a P1200 enclosure
Issue:
How to install the S33576MK and S33576 onto a PowerPacT P frame circuit breaker enclosure

Product Line:
P-frame Breaker Enclosures

Resolution:
For NEMA 1 and 3R enclosures, first install the neutral CT mounting kit piece oriented with the red piece on the bottom and the lugs on the top, with the neutral lug and bonding hole on the left side. For NEMA 4X and 12 enclosures, that piece will be on the bottom. Then mount the other piece next to it, so that the red pieces are back to back, about an inch apart. Then bolt the neutral CT to the mounting kit using the provided studs, with the H2 side on the top. If the breaker enclosure is being used as service entrance equipment, you will also need to install the neutral bonding strap to the top piece using the bonding hole. For more information, see the video below:

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings