Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the Canadian Load Centers, QO2L70RB and QO2L70S Service Entrance Rated?
Product Line:
QO Load Centers

Resolution:
The QO2L70RB and QO2L70S are Service Entrance rated for Canada, when used with ONE  2 pole, QO breaker up to 70 A MAX.
NOTE: If the Load Center is NOT being used for a Service Entrance Application OR is being used for 2 circuits(so QO Tandem breakers or two 1pole breakers) are being used, REMOVE the bonding screw.

Schneider Electric Canada

Attachment(s)
QO2L70RB.JPG.jpg [39.9 KB]
Wording on QO403L100RB and QO2L70RB LC wiring diagrams.xls [26.5 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings