How can we help you today?

Does the Powerpact P frame with IEC only (without UL) rating have Lloyd's of London certification?

Product Line:
Circuit Breakers

Resolution:
When the IEC PP-P is built in North America, it is labeled as a Compact NS breaker, so the Lloyd's cert applies.

Also, the Compact NS630b - 3200A is available in Canada.

Schneider Electric Canada
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
  • Product Selectors