Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are QO and QOB breakers marine UL listed?

Issue:
Are QO breakers Marine labeled?

Product Line:
Breakers

Resolution:
Type QO(B) 10-30 A circuit breakers comply with the marine rating requirements in the UL 489 standard. However, they are not UL marine labeled or certified.

Schneider Electric Canada

Attachment(s)
1072a.pdf [41.41 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings