Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a two pole QO tandem breaker?
Issues:
Are QO 2 pole tandem breakers available?

Product Line:
QO Circuit Breakers

Resolution:
No. You can use two QOT1515 or QOT2020 circuit breakers and a handle tie, QOTHT, for common switching of center two poles, which gives you one two pole (not common trip) and two single poles.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings