How many mounting rail clips are there on QO and QOB breakers?
Issue:
Mounting rail clips information on QO & QOB breakers.
Product Line:
QO & QOB Miniature circuit breakers
Resolution:
The main function of the mounting rail clips is to hold the breaker to the rail of the panel. In the past, some rail clips were made of white nylon plastic. All rail clips are now made of steel. These rail clips are not replaceable.
1 pole breakers have 1 rail clip.
2 pole, 10-30 A have 1 rail clip.
2 pole, 35-125 A have 2 rail clips.
3 pole, 10-30 A have 1 rail clip.
3 pole, 35-100 A have 2 rail clips.
3 pole, QO-VH and QOH, 40-100 A have 3 rail clips.
Mounting rail clips information on QO & QOB breakers.
Product Line:
QO & QOB Miniature circuit breakers
Resolution:
The main function of the mounting rail clips is to hold the breaker to the rail of the panel. In the past, some rail clips were made of white nylon plastic. All rail clips are now made of steel. These rail clips are not replaceable.
1 pole breakers have 1 rail clip.
2 pole, 10-30 A have 1 rail clip.
2 pole, 35-125 A have 2 rail clips.
3 pole, 10-30 A have 1 rail clip.
3 pole, 35-100 A have 2 rail clips.
3 pole, QO-VH and QOH, 40-100 A have 3 rail clips.
Released for: Schneider Electric Canada


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.