Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to purchase an 8903, 30A electrically held lighting contactor with 12 NC contacts?
Issue:
Need to purchase an 8903, 30A electrically held lighting contactor with 12 NC contacts?

Product Line:
8903 Lighting Contactor

Environment:
NEMA Contactors and Starters

Cause:
Normally Closed Contacts Needed

Resolution:
Square D makes a special Class 8903L electrically held contactor with 12NC poles. This is available only from the factory in either Open style, p/n 8903LO0012V02 or in a NEMA 1 enclosure, p/n 8903LG0012V02.  For more information, look at Instruction Bulletin 30072-013-30A.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings