Are the new AF and AFGF circuit breaker load terminals IP2X compliant?
Issue:
Are the load terminals on the AF and AFGF breakers finger safe?
Product Line:
QO and HOM arc fault and dual function breakers
Resolution:
Yes, the lug connectors for the QO and HOM AF and AFGF circuit breakers are IP2X compliant.
Are the load terminals on the AF and AFGF breakers finger safe?
Product Line:
QO and HOM arc fault and dual function breakers
Resolution:
Yes, the lug connectors for the QO and HOM AF and AFGF circuit breakers are IP2X compliant.
Released for: Schneider Electric Canada