Are the new AF and AFGF circuit breakers direct replacements for the old CAFI and DF breakers?
Issue:
Can AF and AFGF breakers be put in the same spot as the CAFI and DF breakers?
Product Line:
QO and HOM arc fault and dual function breakers
Resolution:
Yes, they have the same functionality and fit in the same spots as the old CAFI and DF breakers.
Can AF and AFGF breakers be put in the same spot as the CAFI and DF breakers?
Product Line:
QO and HOM arc fault and dual function breakers
Resolution:
Yes, they have the same functionality and fit in the same spots as the old CAFI and DF breakers.
Released for: Schneider Electric Canada