What is the difference between the S prefix and P prefix shunt trip and UVR part numbers for H, J, and L frame breakers (e.g. S29386 vs P29386)?
Product line:
PowerPact breakers
Resolution:
The S prefix shunt trip and UVR part numbers had screw terminals. These are all being phased out and replaced with P prefix shunt trip and UVR part numbers (the 5 following digits will remain unchanged), which will all have push in terminals. These will always have an aesthetic change, with the newer P prefix part numbers having a darker aesthetic. The form, fit, and function will remained unchanged, and the newer shunt trips/UVRs can be used in older H, J, and L frames and vice versa.
Affected part numbers:
S29384 -> P29384
S29385 -> P29385
S29386 -> P29386
S29387 -> P29387
S29388 -> P29388
S29389 -> P29389
S29382 -> P29382
S29390 -> P29390
S29391 -> P29391
S29392 -> P29392
S29393 -> P29393
S29394 -> P29394
S29404 -> P29404
S29405 -> P29405
S29406 -> P29406
S29407 -> P29407
S29408 -> P29408
S29409 -> P29409
S29402 -> P29402
S29410 -> P29410
S29411 -> P29411
S29412 -> P29412
S29413 -> P29413
S29414 -> P29414
See attached file for more information.
Released for: Schneider Electric Canada