Is the Lug Kit AL800P7K Compatible to Use with MG, MJ, PG, PJ, PK, and PL Molded Case Circuit Breakers?
Issue: Compatibility of Lug Kit AL800P7K with MG, MJ, PG, PJ, PK, and PL Molded Case Circuit Breakers
Product Line: PowerPacT M and P-Frame Molded Case Circuit Breaker
Resolution:
Yes, the lug kit AL800P7K can be used with PowerPacT MG, MJ, PG, PJ, PK, and PL breakers. It has a wire range of (2) 3/0 AWG-750 kcmil and the conductor type should be compact aluminum ONLY.