Are PowerPact breakers with the new green labels compatible with older I-Line panelboards??
Issue:
The new breakers with green labels and Schneider electric branding look different from the old ones with gray labels, do they need additional modifications to be installed into an I-line panels?
Product line:
Powerpact H, Powerpact J, L M P R
Resolution:
No, you won't need to perform any modifications, they are fully compatible.
The updated PowerPact breakers now feature a green label and Schneider Electric branding, which may look different from the older Square D versions with gray labels. However, the form, fit, and function remain the same. These breakers have identical dimensions and electrical characteristics, and no additional hardware or modifications are needed to install them in existing I-Line panelboards.