How can we help you today?

How to Enable and Disable Access to Protection Settings on Micrologic X Control Unit?

Article available in these languages:

  • Spanish

Issue:
How can we restrict access to the protection settings to prevent accidental changes?

Product Line:
Micrologic 5.0X, Micrologic 6.0X

Resolution:

Acess to the protection settings can be enabled/disabled by using the MicroLogic X display screen at Home > Configuration > General > Lock protection

From the Lock protection screen of the MicroLogic X control unit, you can allow changes to the protection settings from the following interfaces:

• Keypad: MicroLogic X display screen keypad itself
• External access: EcoStruxure Power Commission software, EcoStruxure Power Device app, and communication network

For each interface:

• Set as Allowed (factory setting) to enable changes to be made.
• Set as Not Allowed to disable changes.