How can we help you today?

How to adjust the protection settings on Micrologic X control Unit?

Article available in these languages:

  • Spanish

Issue:
The control unit does not have any dials, what are the steps to adjust the protection settings?

Product Line:
Micrologic 5.0X, 6.0X Control Unit

Resolution:
The Micrologic 5.0X and 6.0X control units have a Human Machine Interface; the procedure for the setting protection setting conforms to UL489SE, with an exclusive editing session and a two-step procedure for submitting and applying protection setting changes.

To set a protection setting, access to protection settings must be enabled by using the MicroLogic X HMI. See FAQ FAQ000282170

The following example shows how to set the long-time overcurrent protection:

Steps 1- 7

Steps 8-10