How can we help you today?

What is the current measurement accuracy of the Micrologic X Control Units?

Article available in these languages:

  • Spanish

Product Line:
Masterpact MTZ

Resolution:

MasterPacT MTZ devices with Micrologic X control Unit comply with IEC/EN 61557-12, Class 0.5 accuracy for voltage and current and Class 1 accuracy for active power and energy measurements. For each measurement the accuracy is certified within a temperature range of -25 to 70°C (-13 to 158°F).

The following table indicate the current measurements available and specify the accuracy and accuracy range for different MasterPacT MTZ circuit breakers.

Current Accuracy and Accuracy Range

MicroLogic X Control Unit Measurement Values for voltage, power and frequency are described on the tables from page 32 to 32 of the Catalog 0614CT1701.