Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How can you get a motor running indication from the ATS48 unit?
Issue :
Which Relay contact would you land wires on to get a motor running indication from an Altistart 48?

Product Line :
Altistart 48

Environment :
All

Resolution :
To obtain a contact closure indicating motor is running, could set up relay R3 for rnl which changes state when the motor is powered.
This programming is done in the I/O menu of the parameters.