Naše značky

Impact-Company-Logo-English Black-01-177x54

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the difference between the 9080 MH10 and MHA10 end clamps?

Issue
Customer would like to know the difference between the 9080 MH10 and MHA10 end clamps.

Product Line
Terminal Blocks

Environment
All Products

Cause
Product features and selection

Resolution
The MH10 was for DIN 1 and DIN 3 track and is now obsolete.

The MHA10 is DIN 3 only.


CTA-ID : 2014767