Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the part number for the LED pilot light bulbs used in a Model 6 Drives MCC?
Issue:
Replacement LED pilot light bulbs for Model 6 MCC drives

Product Line:
Model 6 LVMCC

Environment:
All

Cause:
LED replacement

Resolution:
LED Bulb for 22mm type XB5 (plastic) or XB4 (metal), used for 110/120Vac
25501-00003 - Red LED
25501-00005 - Green LED
25501-00004 - Yellow/Amber LED
25501-00006 - Blue LED
25501-00007 - White LED

LED bulb for 30mm 9001 type K, used for 120Vac/dc
6508805210 - Red LED
6508805212 - Green LED
6508805211 - Yellow/Amber LED
6508805213 - Blue LED
6508805214 - White LED