Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Does the 27kV Master-Clad switchgear require a different lift truck than the 5/15kV?

Issue:
Lift truck for 5/15 and 27kV Master-Clad switchgear

Product Line:
MasterClad.

Environment:
Products sold in the United States.

Resolution:
Yes.
For a 5/15kV Master-Clad:
-If the breaker is rated less than 63kA, the part number is 46007-383-50.
-If the breaker is rated 63kA, the part number is 46017-217-50.
For a 27kV Master-Clad, the part number is also 46017-217-50.