Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How many Preset Speeds does the Altivar 61 and 71 support?
Issue:
N/A

Product Line:
Altivar Machines, Altivar 61, Altivar 71

Environment:
All Altivar 61 and Altivar 71

Cause:
N/A

Resolution:
The Altivar 61 and Altivar 71 product line supports up to 16 preset speeds including the Low Speed setting.

Preset speeds can be selected under the Menu 1.7 Application Functions > Preset Speeds, submenu.  Assignments available are:
2 Preset Speeds (PS2)
4 Preset Speeds (PS4)
8 Preset Speeds (PS8)
16 Preset speeds (PS16)

Preset speeds can be triggered using Logic inputs or by changing bits using Communications.  The Preset Speeds can be set from Menu 1.3 Settings or Menu 1.7 Application Function > Preset Speeds.

See the ATV71 Programming manual for the logic chart and more details.