Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is the ATV212 available with bypass?
Issue:
Bypass option on the ATV212.

Product Line:
Altivar ATV212

Environment:
All serial number, all model number

Cause:
Customer wants to know if the ATV212 is available with bypass.

Resolution:
The ATV212 can be ordered as an enclosed package with the bypass option. See the S-Flex drives in the Digest or AC Drives and Soft Starts Pricing Guide to select part numbers.
Here is a link to the ATV212 S-Flex product page where options, dimensions, and other product details can be found.
https://www.se.com/us/en/product-range/61299-sflex-212-drive/#overview ​​​​​​​

Schneider Electric Česká republika

Přílohy
S-Flex Manual 30072-451-83_06.pdf [6.67 MB]