Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What circuit breaker will work with the ATV71 Drive?
Issue:
Breaker recommendation request for an ATV71

Product Line:
Altivar 71

Environment:
All ATV71 models, All Serial Numbers.

Cause:
Customer was unable to find this information

Resolution:
Please refer to the attached document for SCCR ratings and breaker selection for open style ATV71 drives based on UL testing:
https://www.se.com/us/en/download/document/S1B86988/