Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How much extra space is there to the front and rear of the internal rack posts on the NetShelter CX when the rails are at their furthest positions?
Issue:
Customers need to know how much room there is in the NetShelter CX beyond the rails.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Customers want to avoid interference with the front door and rear fan units.

Resolution:
Forward of the front rack posts = 100mm / 4”
Rearward of the rear rack posts = 60mm / 2” (Except, where fan modules intrude there is no usable extra space)