Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Video: Can the ATV212 default display value be changed from output frequency to another value?

Article available in these languages: Španělština

Issue:
Changing the default output value showed on the display.

Product line:
Altivar ATV212

Environment:
All models, all serial numbers

Cause:
Customer preference

Resolution:
Parameter F710 sets the default display.  The factory setting is 0 for motor operating frequency. Other options:
1 = speed reference
2 = motor current
3 = drive rated current
4 = drive thermal state
5 = output power
6 = PID internal speed reference
7 = serial comm data
8 = output speed
9 and 10 are communication frames received data