Jak vám dnes můžeme pomoci?

Can you get an enclosed ATS22 soft starter with a integral full voltage bypass?

Issue:
Enclosed ATS22 soft starter with a integral full voltage bypass.

Product Line:
Altistart ATS22 enclosed

Environment:
All

Cause:
Full voltage bypass option

Resolution:
When you are building up the part number in product selector, choose power circuit Y, to get a integral full voltage bypass option, on the enclosed ATS22 soft starters.