Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How is the ATV61 / ATV71 drive set up for HMI control?
Issue:
Set up for keypad control with ATV61 and ATV71.

Product Line:
ATV61 and ATV71 drives

Environment:
All

Cause:
Running the drive start stop and speed control from the HMI

Resolution:
If normal operation of the VFD is designed for Start/Stop and Reference control to be through the HMI/keypad, program the VFD as follows, under the Drive menu:

1.6 Command menu
Ref 1 channel = HMI
Profile = Separate
Cmd switching = ch1 active
Cmd channel 1 = HMI
Ref 2 switching = ch1 active

1.7 Application Function
Ref 1B switching = ch1 active