Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is RTU Control and which devices support it?

RTU Control is a software tool that may be installed with the Easergy Configurator. The software tool offers a PLC like programming environment supporting several types of programming including: Ladder Logic, structured text, and function block diagrams.
The Flair 200C and T200 support this tool and its programs.