Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is it possible to upgrade the firmware of ATS48 ?

Goals and Symptoms

Is it possible to upgrade the firmware of ATS48 ?
Keywords: revision version Control Board software

Causes and Fixes

Firmware may only be updgraded by changing the Control Board for the latest revision. It is not possible to upgrade the code only.
The version in your Control Board may be read from a label on the top plate.
The Part Number for a spare Control Board is VX4G481.