Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the part number for the ASi bus connector on the TSXSAY100, TSXSAY1000 and the 140EIA92100 modules?

Issue:
ASi bus connector for the TSXSAY100, TSXSAY1000 and 140EIA92100 modules


Product Line:
TSXSAY100, TSXSAY1000, 140EIA92100


Resolution:
We do not have a part number for this connector and cover assemble that the customer can order from SE.
We do have the vendor's part number for just the connector, it is Phoenix Contact number 1841909.
We also can internally order them from France, the part number is W815891970101A.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Česká republika

Zjistěte více
Produkt:
Řada:
Zjistěte více
Produkt: