Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How to copy variables between Vijeo Designer projects

Goals and Symptoms

To inform the user how to copy variable between Vijeo Designer projects using the import and export functions

Causes and Fixes

You can import and export .csv files in the variable database. Using this feature, you can share variables from
one project to another. Another useful feature of the .csv file is that you can manipulate the variable properties in
a spreadsheet program, then import the data into the project again.

IMAGE
Exporting the Variables
image2
image3
3. Click Save


Importing the Variables
image4


Legacy KB System (APS) Data: RESL173992 V2.0, Originally authored by MiOB on 09/04/2013, Last Edited by GeMc on 09/04/2013
Related ranges: Vijeo Designer