Which PLC's are supported by the WINMATE (SFW572) v2.0 and v2.1 programming software?

Article available in these languages: japonština

WINMATE (SFW572) v2.0 and v2.1 programming software supports the following SY/MAX series model controllers:
Models 100, 300, 300D, 400, 450, 500, 600, 650 and 700 series controllers.

Schneider Electric Česká republika