Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
In Vijeo Designer, what changes in the application will require to delete Preserve Runtime Data on download?

    • Changes to recipe or security data while editing the project may cause incompatibility with the run-time data or result in data that cannot be preserved. For example:
        • If any variable is changed while editing the project, even a variable that is not related to the recipes, all recipe data cannot be preserved.
        • If a single recipe is changed (i.e., a change to a recipe's name, ingredient list, or recipe value), all recipe data cannot be preserved.
        • If a recipe group is added to or deleted from a recipe group, all recipe data cannot be preserved.
        • If a recipe group is added, deleted, or changed, all recipe data cannot be preserved.
        • If security data is changed (i.e., a user group is modified), the existing security data on runtime can be preserved but the modified security data will not be downloaded.