Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is it possible to use an output contactor to open the motor circuit on the ATV12?

Issue: Is it possible to use an output contactor to open the motor circuit on the ATV12?

Product Line: ATV12

Environment: All

Cause: ATV12 and Output contactor

Resolution:
The ATV12 has been designed to support this kind of application without any particular precaution (without ferrite...).
So you can add an output contactor directly between the motor and the drive and open it even if the motor is loaded