Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is there a way to print or save a graphic panel page in Vijeo Designer?

Issue:
Printing or saving a graphic panel page in Vijeo Designer


Product Line:
Vijeo Designer


Resolution:
Yes, by using the Panel Report feature of Vijeo Designer. You can save or print the panel pages.
During runtime, you can make use of the Screen snapshot feature and either print to a printer connected to the HMI or save to a file on Secondary or Optional drive.