Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Use of 2 scripts driver on XBTGT2000

Goals and Symptoms

Does the XBTGT2000 allow 2 scripts driver on the COM1 (DB9) and on the COM2 (RJ45)

Causes and Fixes

The XBTGT2000 Series and higher have two communication ports:
- COM1 (DB9 connector).
- COM2 (RJ45 connector).

Both ports allow the target to communicate with a PLC. However, only the COM1 port (DB9) allows the target to communicate with a serial device using the script driver. The RJ45 connector (the COM2 port) doesn't support this script driver.

Unfortunately, this means that it is impossible to connect 2 devices to an XBTGT using two script drivers.


Legacy KB System (APS) Data: RESL176579 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT GT 5.7