Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Which firmware version of ILA2E and ILA2E supports the synchronous operation mode for using in TwinCAT-NC?

Goals and Symptoms

Which firmware version of ILA2E and ILA2E supports the synchronous operation mode for using in TwinCAT-NC?

Causes and Fixes

ILA2E and ILE2E supports the synchronous operation mode from firmware version >=V1.015 (>=RS01).
If the device identification plate shows a lower version, the synchronous operation mode are not supported and cannot be updated !!!