Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What could cause "error during connect" (This isn't a valid PLC Address, or PLC is busy, or media is off.) when connecting to the Unity simulator.

This condition can be caused by a conflict with Ethernet services onboard the PC.
Try deactivating  any Ethernet services such as wireless drivers. If you're using the CyberLogix Ethernet MBX Driver Suite deactivate it and re-launch the Simulator. If you have a Kepware / OPC server running try turning that off.