Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Illumination power for XVBL35 ?

Goals and Symptoms

Illumination power for XVBL35 ?

Facts and Changes

XVBL35

Causes and Fixes

The illumination power (flux) of the LED bulb included in XVBL illuminated beacons with steady light as well as integral flashing light) is 17,7 lumens for the orange colour.


Legacy KB System (APS) Data: RESL197911 V1.0, Originally authored by LaBe on 02/27/2009, Last Edited by LaBe on 02/27/2009
Related ranges: Harmony XVB