Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How long does the biometric switch keeps the storaged records without power alimentation ?

Goals and Symptoms

How long does the biometric switch keeps the storaged records without power alimentation ?

Facts and Changes

Biometric key switch
XB5S

Causes and Fixes

The records are stored in a flash memory. It is comparable to an USB key. There is no battery. It can keep the records for more than a year.


Legacy KB System (APS) Data: RESL197914 V1.0, Originally authored by LaBe on 02/27/2009, Last Edited by LaBe on 02/27/2009
Related ranges: Harmony XB5