Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Zelio Analog: Does galvanic isolation between input (Icom, I1, I2, I3) and output (OPG, Io1, Io2, Vo) device?

Goals and Symptoms

Zelio Analog:
Does galvanic isolation between input (Icom, I1, I2, I3) and output (OPG, Io1, Io2, Vo) device?

Facts and Changes

RMC
Zelio Analog

Causes and Fixes

In the Zelio Analog range, the RMCL55BD, RMCV60BD, RMCA61BD contains isolated modules. The isolation value is about 1.5 Kv.


Legacy KB System (APS) Data: RESL198220 V1.0, Originally authored by LaBe on 04/03/2009, Last Edited by LaBe on 04/03/2009
Related ranges: Zelio analog