Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What would cause the error " E1208 usage of dynamic arrays disabled" in Control Expert (formerly Unity Pro) ?
If your application uses an array, any attempt to access an array member will result in this error. E1208, take the following action to eliminate the error.

Go to Tools/Project Settings/Variables
Select "Allow Dynamic Arrays  ANY_ARRAY_XXX)"
Select "Directly represent array variables"
Select OK and Build Changes.



R-122018

Legacy KB System (APS) Data: RESL210281 V1.0, Originally authored by DaSo on 01/10/2013, Last Edited by DaSo on 01/10/2013
Related ranges: Unity Pro - SoCollaborative software