Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the part number for the PM810, PM820, PM850, and PM870 meter remote display kit?

Issue
Part number for PM800 series remote display kit

Product Line
PM800 series

Environment
Part Numbers

Resolution
The part number for the PM800 series meter remote display kit is PM8RD. This part number includes the remote display, the cable (CAB12) and the 4-wire, RS232/485 communication module.
Please note there is no commercial part number for just the remote display itself. The part number for the PM800 series meter remote display adapter is PM8RDA.

The PM800 series has passed the end of commercialization period and therefore distributors may or may not carry the parts.