Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Can I use my 8600 Form 9/9S meter with a different Volts mode/wiring scheme?

The 8600 meter is very versatile in its ability to be altered. If you look at the Installation Guide you will notice many form factors and wiring schemes in each.
The wiring schemes for other form factors can be used for your meter as long as two requirements are met:

  1. The necessary Voltage/Current inputs exist
  2. The Volts mode (in the basic setup) is matched to the wiring scheme you are using