Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How to interpret the manufacturing date code on a PowerLogic Enercept Meter
Issue:
How can I tell when my Enercept meter was manufactured?

Product:
Enercept Meter

Environment:
Power Metering

Resolution:
The date code on the Enercept meter appears in the following format:
Date Code: 201120

This code is translated into the 20th week of the year 2011. The first four digits are the year of manufacture and the last two digits are the week of manufacture for that year.