Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What ports are used by Vijeo Designer v4.5 to download an application via TCP/IP?

The following Ports are used by VD v4.5 to download an application via TCP/IP:
21 FTP
6001 Programming port
6002 Programming port
8000 Used for data sharing and Web Gate
13777 Alternative to port 21

Note: Not all Magelis terminals use all of these ports. However VD will try to establish a connection with all of them.
If the terminal does not use one or more of these ports then the connection will be ignored.