Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How to round up value when displaying data log in ION Enterprise, SPM, and PME Vista

Issue:
The customer does not want accuracy higher than whole number values.

Product Line:

ION Enterprise
StruxureWare Power Monitoring (SPM)
Power Monitoring Expert (PME)

Environment:
Vista Data Log Viewer
Web Applications Data Log Viewer

Cause:
Software rounds to the thousandth place.

Resolution:
Confirm that Show Toolbox is checked in Options in the top-left then right-click on the data log viewer that needs to be changed in Vista. Go to the Query tab and click Edit SQL ... Add a ROUND function to the queries, for example

SELECT timestamp
, "Vll ab mean"
, "Vll bc mean"
, "Vll ca mean"

becomes

SELECT timestamp
, ROUND("Vll ab mean", 0) AS "Vll ab mean"
, ROUND("Vll bc mean", 0) AS "Vll bc mean"
, ROUND("Vll ca mean", 0) AS "Vll ca mean"

Save the file. Double-click on the data log viewer and you should see the value is rounded up to the nearest integer.