Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
When the front panel of the CM2 reads 999,999 MWh, what happens at the front panel when the MWh continue to increase? Does the CM2000's energy reading roll over?

Issue
User would like to know what happens when energy reading of the CM2000 increases beyond 999,999 MWh with respect to the front panel display

Product Line
CM2000

Environment
Front panel

Resolution
The front panel display will roll over from 999,999 MWh to 000,000 MWh.
If reading Wh from front panel you would need to note that a roll-over has taken place. Also note that the LED next to Mega stays lit after the roll-over has occurred.