Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Troubleshooting GPS time Synchronization on ION meters

Issue
Customer has difficulties time synchronizing an ION meter with the GPS receiver.

Product Line
ION metersTime synchronization

Resolution
- Check whether the Clock Source setup register is set to COMMS.
- Check whether correct communication port has been selected through the Time Sync Source setup register.
- Finally, check in the Communication module whether the receiver that you want to use is correctly selected from the Protocol setup register.
- Make sure the from the front panel of the meter the hardware mode is selected to RS485 or RS232. Front panel>>COM>>hardware>>Mode>

for more information, Please refer to Time Synchronization & Timekeeping document .